Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number of the drop out pads for an 8502 or 8536 SE or SF (size 3 or 4) magnetic contactor or starter?
Issue:
Replacement drop out pads for 8502/8536 starter

Product line:
NEMA Contactors and Starters

Environment:
8502/8536 Contactors and Starters

Resolution:
Part number 3109115701 for a NEMA Size 3 or 4. Two pads are required per device.

If red / orange drop out pads are installed make sure to remove the entire drop out pad before installing the new style black bumpers

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings