Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the options available on a 14 inch wide NQ three phase panelboard?
Issue:
Are they available in NEMA 3R, split bus or with internally installed contactor?

Product Line:
NQ Panelboards

Environment:
Products sold in North America

Cause:
14" wide NQ panelboard special features?

Resolution:
No. There are no options available for 14 inch NQ panels for NEMA 3R enclosure, split bus or installed lighting contactor.
These are available in standard NEMA 1 indoor enclosures only without any special options.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings