Issue:
How to select a Tesys SK Control Relay?
Product Line:
Industrial Relays
Environment:
TeSys SK IEC Relays
Cause:
Application is calling for a different voltage to control the relay.
Resolution:
The CA2SKE20** alternating relays are available in the following voltages:
The ** is filled in with the appropriate voltage code from the table above, for example a 24VAC coil will be CA2SKE20B7
How to select a Tesys SK Control Relay?
Product Line:
Industrial Relays
Environment:
TeSys SK IEC Relays
Cause:
Application is calling for a different voltage to control the relay.
Resolution:
The CA2SKE20** alternating relays are available in the following voltages:
| Voltage | 24 | 48 | 120 | 220 | 240 | 480 |
| 50/60 Hz | B7 | E7 | G7 | M7 | U7 | T7 |
The ** is filled in with the appropriate voltage code from the table above, for example a 24VAC coil will be CA2SKE20B7