Issue:
Can you use a QO-GFI, QO-EPD, QO-EPE breaker on a QO3100BNF/S or QO3100BNRB enclosure?
Product Line:
Miniature circuit breakers and enclosures
Resolution:
Yes, but only in current design series 003, available from February of 2010. The series number can be identified on the package label or the device's wiring diagram. These breakers should not be used in any device with earlier series numbers.
Can you use a QO-GFI, QO-EPD, QO-EPE breaker on a QO3100BNF/S or QO3100BNRB enclosure?
Product Line:
Miniature circuit breakers and enclosures
Resolution:
Yes, but only in current design series 003, available from February of 2010. The series number can be identified on the package label or the device's wiring diagram. These breakers should not be used in any device with earlier series numbers.
Released for: Schneider Electric Canada