Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part # for the Harmony Biometric Switch?
Issue:
Selecting right part number for XB5S Biometric switches.

Product Line:
Push Buttons and Operator Interface

Environment:
XB5S Biometric Switches

Resolution:
For a maintained/bistable switch select the XB5S1B2L2 (pre-wired 2 m cable) or XB5S1B2M12 (M12 connector).
For a momentary/monotstable switch select the XB5S2B2L2 (pre-wired 2 m cable) or XB5S2B2M12 (M12 connector).
For a maintained/bistable USB switch select the XB5S3B2L2 (pre-wired 2 m cable) or XB5S3B2M12 (M12 connector).

For a momentary/monotstable USB switch select the XB5S4B2L2 (pre-wired 2 m cable) or XB5S4B2M12 (M12 connector).
USB biometric switch dedicated to Schneider HMI 24Vdc select the XB5S5BL2L.


See Pricing Guide 9001PL0901 for accessories.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings