Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are box lugs available on the 20, 25 and 30 amp 8910DPA contactors?
Issue:
Box lugs for 8910DPA 20A, 25A and 30A rated

Product Line:
NEMA and Definite Purpose Contactors and Starter

Environment:
8910 Definite Purpose Contactor

Resolution:
On 20, 25 and 30 amp devices we would previously use Form Y124 (see note below). Devices rated 40 amps and larger are provided as standard with box lugs.

Note: There are no field modification kits available for this conversion. Y124 (Copper box lugs) is an obsolete option with the new Series C 8910DPA 20,25,30 amp contactors. Only Y239 (Aluminum box lug) option is available

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings