Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are single phase main breaker I-Line panels constructed with two pole or three pole main breakers?

Issue:
Design for single phase main breaker

Product Line:
Panelboards

Environment:
I-Line Power Distribution Panelboards

Resolution:
Because there are 3 poles on the busbar, main breaker I-Line panels always use 3 pole breakers, whether single phase or three phase. For single phase panels, only A and C phases are connected to the utility power. The B or center phase is used only as a spacer.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings