Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Adding a CE3200B to an existing CDP panel

Article available in these languages: Spanish

Issue:
Obsolete breaker cross

Product Line:
Circuit breakers


Resolution:
The CE3200B breaker is obsolete.
The Replacement breaker is a Square D JDL36200 breaker with a JDCMH mounting kit. This breaker is rated 14KAIC at 600V.
The JDCMH will mount two J frame breakers.
An S37445 is included in the JDCMH to convert breaker from Lug-Lug to Lug-Pad. If a second breaker is being mounted on the JDCMH Hardware, order an additional S37445.
Hardware Kit requires both sides of panel and will only mount Powerpact J Breakers.


Schneider Electric Canada

Attachment(s)
JDCMH 32-02-211a-00x.pdf [123.67 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings