Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the Homeline (HOM) and QO load centers available in NEMA 12 or NEMA 4X stainless steel enclosures (boxes)?

Article available in these languages: Spanish

Issue:
Product design features

Product Line:
Load Centers Materials

Environment:
QO or Homeline Load Centers

Resolution:
No. QO and HOMELINE load centers are unavailable in NEMA Type 12 and NEMA Type 4X stainless steel enclosures. They are ONLY available in cold-rolled (NEMA 1) or galvannealed ​(NEMA 3R) steel enclosures. Consider an NQ panelboard for a NEMA 12 or NEMA 4X application.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings