Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement external on/off operator for a 2510FR1, 2510FR2, 2510KR1, or 2510KR2?
Issue:
Replacement handle kit to replace the existing external toggle for Class 210 Types FR and KR.

Product Line:
Manual Starters and Switches

Environment:
Class 2510 Types FR and KR (NEMA 7&9) manual starters and switches

Resolution:
9998HR2 replacement handle or toggle kit for Series B only. Series A is obsolete with no replacement.
The kit includes the following parts:
  • Handle Assembly (includes shaft and toggle button (assembled)
  • "O" Ring
  • Spring Pin (roll pin)

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings