Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the NEMA rating for the GV7AP rotary handles?
Product Line:
Tesys GV Manual Starter and Protectors

Resolution:
These handles do not have NEMA ratings, only IP ratings.
The GV7AP01 and GV7AP02 are IP55 rated.
The GV7AP04 and GV7AP03 are IP40 rated.
And the GV7AP5 is IP43 rated.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings