Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the current rating and wire size for the built-in auxiliary contacts for the LC1D09-D32 contactors?

Article available in these languages: Korean

Issue:
What is the current rating for the built in contacts on the LC1D09-D32 contactors?

Product Line:
IEC Contactors and Starters

Environment:
Tesys D-line contactors

Cause:
Auxiliary contact rating identification

Resolution:
It is 10A continuous (not make and break) and terminals will accept # 18 to # 10 gauge Cu wire.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings