Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
8965 Type R hoist contactor Auxiliary contact part numbers
Issue:
What is the part # for an aux contact used on 8965RO Hoist Contactor?

Product Line:
Contractors and Starters

Environment:
North American Products

Resolution:
Yes, order the 9999R10 for normally open or 9999R11 for normally closed. The contact blocks mount between the forward and reversing contactors. You can only install 1 contact block per 8965RO10 device. The 9999R blocks actually contain either 2 NO or 2 NC contacts in the module, one for each side of the device.

Check for availability

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings