Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the temperature range for a 9001K operator?
Issue:
Identify the operating temperature for a 9001K operator

Product Line:
9001K 30mm Push Button

Environment:
Pushbutton and Operator Interface

Resolution:
The temperature is -25 to +70 °C operation, -40 to +70 °C storage.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings