Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU463DS, series F5? (may be shown as F05)

!!!Confidential ContentIssue:
Repair Part

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the HU463DS, series F5 (F05) are as follows. No other parts are available.
Line Base - one each of 4056776750 (left side base), 4056776150 (right side base), and 4056702801 (plastic connecting cam) (NOTE: arc suppressor not included)
Line Base mounting screw - 4020515101 (3 required per line base)
Arc Suppressor Assembly - HAS0610F (2 required; includes arc suppressor and mounting screw)
Lug assembly - CL10F (includes 6 lugs)
Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
Handle Coupling - 4056699850
Cover Interlock Defeat Coupling - 4056699750
Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
Lockplate mounting screw - 2194900001 (2 required)
Ground Lug - 4025101851 (2 required)
Ground Lug Mounting Screw - 4020514801

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings