Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are NQ panels with feed through lug feature, supplied with feed through ground lugs?
Issue:
NQ panels with feed through lug feature and feed through ground lugs

Product Line:
NQ Panelboard

Environment:
Product features

Cause:
Clarification

Resolution:
There is no feed through ground lug option, nor is it included with the Feed thru lug features.
The ground bar is bolted to the box. An additional QO70AN , Q1100AN, or Q1150AN lug can be added to supplied ground bar, based upon  wire size exiting Panel

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings