Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are replacement contacts available for Class 8903 Type L and LX contactors?
Issue:
Are replacement contacts available for Class 8903 Type L and LX contactors?

Product Line:
8903 type L and 8903 type LX lighting contactors

Environment:
Products sold and used in the United States

Cause:
Replacement contacts are needed for 8903 type L or LX lighting contactor

Resolution:
Yes, 9998RA5B for Type L (SeriesC) or Type LX (Series B and SERIES C). 9998RA5 for Type LL, Type L (Series A,B) and Type LX (Series A).

Note: 4 pole kit, order number of kits based on number of contactor poles. Example, 8903LO1200 would require 3 kits.
9998RA5B should fit the series C contactor.


CTA-ID : 2054265

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings