Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will a PowerPacT H frame with a GFM150HD ground fault module fit into an HCN I-Line panel?
Issue:
GFM150HD ground fault module into an HCN I-Line Panel

Product Line:
Panelboards

Resolution:
No. You must use at least an HCP type panel to fit the GFM module into it, since the module adds 4.85" to the length of the breaker.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings