Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a QMB362T21W, Series E1 (E01)?
Issue:
Repair parts

Product Line:
QMB branch Switch

Resolution:
The QMB device is a twin switch, meaning it contains two switches in the one device. One side is 30 A, the other is 60 A. Parts are listed per switch. Only the parts listed below are considered field replaceable:
Arc Shield/Suppressor Assembly - 4051239950 (1 required)
Load Base Assembly 60 A - 4051241150 (1 required; includes lugs)
Load Base Assembly 30 A - 4051242550 (1 required; includes lugs)
Load Base Mounting Screw - 4020506501 (2 required per load base)
Handle Knob Kit - 4028343750
Lug Assembly - 4025101652 (per lug)
Lug Mounting Nut - 2342702001 (per lug)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings