Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are 9013F pressure switches lead free? Are these Residential Water Pump Switches certified NSF-61 and NSF 61 Annex G?

Issue:
Are the 9013 type F pressure switches lead free, and are they certified NSF-61 and NSF 61 Annex G

Product Line:
Pressure Switches

Environment:
Class 9013 type F pressure switches

Cause:
Are the 9013 type F pressure switches lead free, and are they certified NSF-61 and NSF 61 Annex G


Resolution:

The entire line of 9013 F Water Pump Pressure Switches are certified NSF-61 and NSF 61 Annex G for Drinking Water System Components - Health Effects. Certification is for the Water Contact Material. NSF 61 Annex G is a third party certification for California Assembly Bill AB1953.``

California Bill is Assembly Bill No. 1953 is available on line. Search for its locations on Google

See brochure 9013HO0901R01/10 for more information

Below is the address for the published confirmation.

http://www.nsf.com/Certified/PwsComponents/Listings.asp?Company=C0028348&Standard=061


CTA-ID : 2054422

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings