Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the standard lug on a SN400LA neutral assembly?
Issue:
What is the standard lug on an SN400LA neutral assembly?

Product Line:
Molded Case circuit breakers and accessories

Environment:
Selection

Cause:
Installation

Resolution:
The standard lug provided on the SN400LA is an AL400LA. The AL400LA Lug will only accept (1) #1AWG-600 kcmil or (2) #1AWG-250 kcmil CU or AL conductors.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings