How can we help you today?

What are the repair parts for an H226, series E2 or E4?

Product Line:
Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN226E2 (includes line and load base assembly, arc suppressor assembly, box insulator, line phase insulators, and mounting hardware)
Line base assembly - 4055218550SEL (2 required; arc suppressor assembly not included)
Load base assembly - 4055218750SEL (2 required)
Arc suppressor assembly - 4051270850 (2 required)
Lug assembly - 4405044601 (2 required per base assembly)
Line base phase insulator - 4051201401 (1 required)
Load base phase insulator - 4055219101 (1 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250SEL
Door thumb retainer - 4405049001
Door thumb screw - 4405043401
Handle knob kit - 4401142750 for series E2, 4028343550 for series E4
Cross Arm Insulator – (2) 4055217701 (left and right side pieces); (1) 4055217801 (center piece); (1) 4055215701 (dust shield – retainer for insulators)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: