Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a H466 Series E2 and E4 Heavy Duty Safety Switch?

Issue:
Repair parts for H466 Series E2 and E4

Product Line:
Safety Switch

Environment:
Heavy Duty Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN466E2 (includes line & load base assembly, arc suppressor assembly, Box insulator, line phase insulators, and mounting hardware)
Line base assembly - 40552-185-50 SEL (4-required and arc suppressor assembly is not included)
Load base assembly - 40552-187-50 SEL (4 required)
Arc suppressor assembly - 40512-708-50 SEL (4-required) Obsolete and replaced by 40512-708-50 (4-required)
Lug assembly - 44050-446-01 (2 required per base assembly)
Line base phase insulator - 40512-014-01 (3 required)
Load base phase insulator - 40552-191-01 (3 required)
Line & load base mounting screws - 40206-009-01 (2 required per base assembly)
Handle assembly - 40512-172-50 SEL
Door thumb retainer - 44050-490-01
Door thumb screw - 44050-434-01
Handle knob kit (black & red knob at end of handle) - Series E2 is 44011-427-50, Series E4 is 40283-435-50

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings