Issue:
Product Design Features
Product Line:
Heavy Duty Safety Switch
Resolution:
The repair parts for the H364SS, series F6 (F06) are as follows. These are the parts that can be replaced. No other parts are replaceable.
-Complete Line Base - 4056703450 (1 required - includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
-Line Base mounting screws - 4020514202 (6 required per line base)
-Load Base Assembly - 4056677450 (1 required per phase; includes phenolic base, lugs, and fuse clips)
-Load Base mounting screws - 4020514202 (2 required per load base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (note: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056718850
-Switch Mechanism mounting screws- 2194918121 (2 required)
-Handle Assembly - 4056896150 (also recommend replacing lockplate gaskets)
-Lockplate - 4056738901 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate mounting screws - 2194918121 (2 required)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801
Product Design Features
Product Line:
Heavy Duty Safety Switch
Resolution:
The repair parts for the H364SS, series F6 (F06) are as follows. These are the parts that can be replaced. No other parts are replaceable.
-Complete Line Base - 4056703450 (1 required - includes phenolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips)
-Line Base mounting screws - 4020514202 (6 required per line base)
-Load Base Assembly - 4056677450 (1 required per phase; includes phenolic base, lugs, and fuse clips)
-Load Base mounting screws - 4020514202 (2 required per load base)
-Arc Suppressor Assembly - 4056677550 (1 required per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - 4025116251 (per lug)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (note: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056718850
-Switch Mechanism mounting screws- 2194918121 (2 required)
-Handle Assembly - 4056896150 (also recommend replacing lockplate gaskets)
-Lockplate - 4056738901 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required) - Obsolete. Replaced with 4050322803
-Lockplate mounting screws - 2194918121 (2 required)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801
Released for: Schneider Electric Canada