Issue:
Repair parts for H226NAWK Series E2
Product Line:
Safety Switch
Environment:
Heavy Duty Safety Switch
Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN226NAE2 (includes line & load base assemblies, neutral assembly, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line base assembly - 40552-214-50 SEL (2 required and arc suppressor assembly is not included)
Load base assembly - 40552-215-50 SEL (2 required)
Arc suppressor assembly - 40512-708-50 SEL (2-required) Obsolete and replaced by 40512-708-50 (2-required)
Lug assembly - 40256-024-50 (2 required per base assembly)
Neutral assembly - H600SNC
Line base phase insulator - 40512-014-01 (1 required)
Load base phase insulator - 4052-191-01 (1 required)
Line & load base mounting screws - 40206-009-01 (2 required per base assembly)
Handle assembly - 40512-172-50 SEL
Vault handle - 40512-194-50 SEL
Handle knob kit (black & red knob at end of handle) - 44011-427-50
Neutral bonding strap - 40283-253-50 SEL
Released for: Schneider Electric Canada