Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the DTU363DS, series F6 (may be shown as F06)?
Issue:
Design Repair parts

Product Line:
Double Throw Safety Switch

Resolution:
The repair parts for the DTU363DS, series F6 (F06) are as follows. No other parts are available.
-Line Base - 4056624750 (1 each upper and lower; arc suppressor and wire assembly not included)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Wire Assembly- 4056780050 (for A and B phase only; includes cable factory connected mechanical lug at one end and a crimped connector at the other end)
-Wire assembly-4056780051 (for C phase only; includes cable factory connected mechanical lug at one end and a crimped connector at the other end)
-Line and Load Lug Assembly - 4025101851 (3 per base assembly)
-Line and Load Lug mounting screw - 4020514202 (1 required per lug)
-Ground Lug(s) - 4025101851 (per lug)
-Ground Lug mounting screw - 4020513503 (1 per ground lug)
-Switch Mechanism - 4056646950 (1 each for upper and lower)
-Linkage Assembly - 4056665350
-Linkage Assembly mounting screws that go into the side of the enclosure- 2194900001 (3 required; also replace the mounting screw rubber gaskets)
-Linkage Assembly mounting screw rubber Gaskets - 4050322802 (3 required)
-Linkage Assembly mounting screw that go into the back mounting pan inside the switch - 2142217101 (4 required)
-Handle - 4056688850
-Lockplate - 4056689501
-Lockplate mounting screws - 2194900001 (2 required; also requires rubber gasket)
-Lockplate mounting screw rubber gasket - 4050322802

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings