Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the wire range for HCP326812N?

Issue:
Cable size allowed

Product Line:
Panelboards

Environment:
I-Line Power Distribution Panelboards HCP

Cause:
Wiring Installation

Resolution:
The wire range is 4 - 3/0 - 500 kcmil al or cu. However the actual lug range is (4) 3/0 - 750 kcmil al or cu. If the wire range required is larger than 500 use the NEC table to determine how many inches of wire bending space is required. Add the required wireway to the panel to allow for the extra wire bending space.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings