Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the Class 2510 Type KO2 and the Type KO6?
Issue:
Class 2510 Type KO2/KO6 difference

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
2510 Manual Starters

Resolution:
Horsepower ratings at 460 and 575 volts are higher for 2510K06. The KO2 is 10Hp @ 460v or 575v, the KO6 is 15Hp @ 460 and 20Hp @ 575.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings