Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are 3 phase QO load centers available with feed thru lugs?
Issue:
Selection

Product Line:
QO Load Center

Resolution:
No. However, feed thru lugs are offered on a select few SINGLE phase QO and HOMELINE load centers. For an application requiring feed thru lugs on a 3 phase panel, consider using a NQ panelboard.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings