Issue:
8910DPA with NC contacts
Product Line:
Definite Purpose Contactors
Environment:
Types DP, DPA
Resolution:
The 8910`s can come with NC contacts ONLY with 4 pole devices and limited to 8910DPA14, 24, and 34. Also, it needs to have form Y392 for it to have 2NC contact out of the 4 poles. The 8910 DPA contactors cannot be field converted from NO to NC.
8910DPA with NC contacts
Product Line:
Definite Purpose Contactors
Environment:
Types DP, DPA
Resolution:
The 8910`s can come with NC contacts ONLY with 4 pole devices and limited to 8910DPA14, 24, and 34. Also, it needs to have form Y392 for it to have 2NC contact out of the 4 poles. The 8910 DPA contactors cannot be field converted from NO to NC.
Released for: Schneider Electric Canada