Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the pin that comes with the 9422ATDN601 disconnect switch?
Issue:
Is the cotter pin on the 9422ATDN601 disconnect switch available as a spare parts?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
9422 Disconnect Switches

Resolution:
The cotter pin part number is 24201-08400. It comes standard in the parts bag # 31055-509-55. It is 1/8 X 1 1/4 inches long.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings