Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the DTU363AWK, series F6? (may be shown as F06)
Issue:
Current design repair parts

Product Line:
Double Throw Safety Switches

Resolution:
The repair parts for the DTU363AWK, series F6 (F06) are as follows. No other parts are available.
-Line Base - 4056624750 (1 each for upper and lower; order load lugs, arc suppressor, and wire assembly separately)
-Line Base mounting screws - 4020515101 (3 required per line base)
-Arc Suppressor Assembly - 4056635550 (1 required per line base)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Wire Assembly - 4056780051 (1 required; includes mechanical lug at one end, cable, and a crimped connector at other end; uses mounting screws of line/load lugs)
- Wire Assembly - 4056780050 (2 required; includes mechanical lug at one end, cable, and a crimped connector at other end; uses mounting screws of line/load lugs)
Lug assembly - 4025101851
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101851 (per lug)
-Ground Lug mounting screw - 4020513503 (1 per lug required)
-Switch Mechanism - 4056646950 (1 each for upper and lower)
-Linkage Assembly - 4056682750 (also replace linkage assembly rubber gaskets)
-Linkage Assembly Rubber Gaskets - 4050322801 (3 required)
-Linkage Assembly mounting screws - 2299940562 (7 required)
-Handle - 4056688750 (handle gasket also required; lockplate gasket may also need replacing)
-Handle gasket - 4056608601
-Lockplate - 4056673301 (lockplate gasket also required)
-Lockplate gasket - 4056608601 (1 required)
-Lockplate mounting screws - 2299940562 (2 required)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings