How can we help you today?

Are Micrologic trip H, J, and L frame breakers available in 2 pole versions?

Product Line:
Circuit Breakers

Resolution:
No, but 3 pole breakers with these trip units can be used for 2 pole applications (2 legs of a 3 phase system), though not always for single phase applications (must be labeled for single phase).