Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum number of AFI breakers in an NQ panelboards?
Issue:
Maximum number of AFI breakers in an NQ panelboards

Product Line:
PTFDS - FD Enclosure Systems

Environment:
NQ panelboards sold and used in North America

Cause:
Determination of total quantity of arc fault breakers that can be installed in an NQ panelboard.

Resolution:
Maximum is (28) per the product selector because of pigtails not being able to reach the neutral.
However, pigtails can be spliced in the factory and in the field,  more than 28 can be installed.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings