How can we help you today?

Is there a contact block like the 9001KA1 that has two normally closed contacts on it?

Issue:
Is there any 2 NC Auxiliary contact for 30 mm Push buttons?

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony 30 mm 9001 K/SK Plastic Push Buttons

Resolution:
No, do not offer.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings