Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is included in the NF250FTL 250 A feed through lug kit?

Issue:
Verifying what parts are included with the NF250FTL.

Product Line:
Panelboard.

Resolution:
The parts in the NF250FTL kit include:
(1) Neutral lug.
(3) Feed-through lugs
(6) 10-32 x 5/16 in tapping screws
(1) 1/4-20 x 9/16 in tapping screw
(3) 1/4-20 x 3/4 in tapping screws
(2) 10-32 x 7/16 tapping screws
(2) Rail extensions
(2) Rail splices
(1) cover extension (2) Deadfront support brackets.

See instruction bulletin 80043-757-02 for step by step installation instructions.
NF250FTL

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help and Contact Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings