Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
HCR548612U: what is the lug wire size for the incoming conductors?
Issue:
Incoming conductor size for HCR 1200A panel

Product Line:
Panelboards

Environment:
I-Line HCR

Cause:
Installation

Resolution:
The lugs are rated for 4 - 3/0 thru 750kcmil cables but the UL wire bending range for the interior and box limits cable to 4-3/0 thru 500kcmil

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings