Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the Kirk keylock order numbers and drawing numbers for the vertical and horizontal mounted locks on Powerpact M, P, and R frame breakers?
Product Line:
Powerpact M, P, R breakers

Resolution:
Kirk Single Lock (horizontal mount) KFL003710** (Square D Drawing # 48186-220-50)
Kirk Single Lock (vertical mount) KFL003710 (Square D Drawing # 48185-267-01)
Kirk Double Lock (vertical mount) KFL003720 (Square D Drawing # 48185-266-01)
Kirk Double Lock (horizontal mount) KFL003720** (Square D Drawing # 48186-224-50)
**requires 3" roll pin

Schneider Electric Canada

Attachment(s)
Kirk Lock Order Form.pdf [76.07 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings