Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I run an ATS softstarter without a motor load or motor connection?
Issue:
Customer wants to test the softstart without a motor

Product Line:
ATS01
ATS22
ATS48
ATS480

Environment:
No Motor connected

Cause:
Trips on PHF

Resolution:
It is not possible to run the ATS softstart  with out a motor connected.
Softstarts use SCR's to switch the voltage on and off to the motor.
To properly fire (switch on) the SCR's there must be some current flow.
Since testing without a motor means there will be no current, the SCR's won't actually be switch on and off properly so it will not be a valid test.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings