Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the replacement hinge on a 8998CP03 Model 6 MCC cover plate?

Issue:
What is the part number for the replacement hinge on a 8998CP03

Product Line:
Motor Control Centers MCC

Environment:
Products sold in North America

Cause:
When moving, adding, or removing MCC buckets, often times a gap occurs that needs a cover plate, or parts for it.

Resolution:
The 3 inch Tall 8998CP03 covers do not come with hinges.  The 8998CP06,  6 inch high, and taller cover plates have hinges . The 8998CP03 cover plate screws directly onto the structure.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings