Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do the current design QO and Homeline Main Breaker Load Centers have a UL listed Two tier or Three tier short circuit current series rating?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
QO and HOMELINE Load Centers

Environment:
Short Circuit Current Series Ratings

Cause:
Application

Resolution:
SCCR's = Short Circuit Current Ratings
2T = Two Tier
3T = Three Tier
'22k-10k' = Two Tier SCCR from Main(22k) to Branch(10k)
'25k-10k' = Two Tier SCCR from Main(25k) to Branch (10k)


Yes, there are 2T and 3T UL SCCR's listed for the QO and HOMELINE load centers.
The 2T SCCR is located on the Box label inside the load center enclosure and the 3T SCCR label is located on the load center cover. These labels will show all the appropriate 2T and 3T UL listed Series Short Circuit Current Ratings(SCCR) for either an integral or remote(upstream) protection with the load center branch breakers. Also, attached is a pdf data bulletin( document # 4100DB0301R03/14 )for the load center Short Circuit Current Ratings.

Two TIER SCCR's:
1) QO and Homeline Single Phase Main Breaker Load Centers supplied with a QOM1-VH (125A max) or QOM2-VH (225A max) main breaker are rated '22k-10k' SCCR Maximum standard, as a 2T SCCR.

2) QO Three Phase Main Breaker Load Centers supplied with a QDL main breaker are rated '25k-10k' SCCR Maximum standard, as a 2T SCCR.
NOTE: The factory installed QDL main breaker can be replaced with a QGL '65k-10k' SCCR or QJL '100k-10k' SCCR Main Breaker.



Schneider Electric Canada

Attachment(s)
4100DB0301R0314.pdf [2.31 MB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings