How can we help you today?

Do Q1 circuit breakers have Visi-Trip windows?

ISSUE
Do Q1 circuit breakers have Visi-Trip windows?

RESOLUTION
Q1 ad Q1-VH from 1979 forward have Visi-Trip windows.  Prior to 1979 they did not have visi-trip windows.
Visi-trip is a feature of the breaker that displays a red/orange flag when the breaker is in the tripped positon.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: