Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What form replaces the H10 or H20 forms for the Motor Logic solid state overload relays?
Issue:
What form replaces the H10 or H20 forms for the Motor Logic solid state overload relays?

Product Line:
NEMA starters, contactors, combination starters, pump panels, reversing starters

Environment:
8502,8536,8538,8539,8702,8736,8738,8739,8940

Cause:
Obsolescence of class 10 and class 20 solid state overload relays

Resolution:
Replace the H10 or H20 form with H30 to select the feature unit, which is selectable between Trip Class 10 and Trip Class 20.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings