Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a manual over ride on the 8903PB panel board lighting contactors?
Issue:
Manual Override 8903PB

Product Line:
Panel board style lighting contactors

Environment:
8903PB

Cause:
Product features
Resolution:
There is a metal piece that is provided in the vertical slot on the front of the contactor. The metal piece has a hole in it.
You can insert an allen wrench to manually open and close the power poles on the contactor.
This will manually override any other control device in the control circuit such as a timer, relay or other controls.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings