Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is remote (electrical) operation possible for the Powerpact RG (R Frame) circuit breakers?
Issue:
Can Powerpact RG (R Frame) circuit breakers be remotely operated?

Product Line:
Circuit Breakers

Environment:
Powerpact RGF, RJF, RKF, RLF circuit breakers

Cause:
Electrical operation of circuit breakers is a common request

Resolution:
Powerpact R frame circuit breakers do not have an electrical operation option.  They may be equipped with a shunt trip (open coil) but they do not have an option for a motor or close coil.
For remote operation of circuit breakers larger than 1200 A, it is necessary to use the Masterpact NW or MTZ with appropriate accessories.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings