Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Terminal Lug Data for ALL the current design series, US and Canada, Double throw safety switches and are there alternate lugs?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
Double Throw Safety Switches

Environment:
Wire size and range for Line and Load lugs

Cause:
Application

Resolution:
DTSS = Double Throw Safety Switches

See below the table for the terminal lug data and any potential alternate lugs, for ALL the current design series DTSS. If alternate lugs are not shown in the table, that means there are NO alternate lugs available.
NOTE: Table 3.56 below, first row information '30 A (Series T4)' is for the 92000 Switch catalog numbers - 92251, 92351 and 92451
Digest tables

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings