Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why has the LIM (line isolation monitor) gone into alarm?
Issue:
Troubleshooting

Product Line:
Hospital Isolated Power Systems

Environment:
NFPA 99, NEC 517.160

Cause:
Exceeding the predetermined threshold of leakage current (2 or 5mA) for an isolated power system will result in LIM alarm.

Resolution:
Among the most common reasons for line isolation monitor alarms are medical equipment failure, damaged extension cords and too many devices plugged into the system.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings