Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a QO-HM breaker available for a 22 kAIC application?
Issue:
Is there a QO-HM breaker available for a 22 kAIC application?

Product Line:
QO-HM single pole breakers

Resolution:
The QO-HM breaker is rated for 10 kAIC. In order to get the QO-HM breaker with 22 kAIC, order a QO115VHHM (1p, 15 A) or QO120VHHM (1p, 20 A).

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings