Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What hardware is required to add an M340/M580 expanded backplane?

Adding an expansion rack requires an Extension rack Module (BMXXBE1000), Extension rack Cable and Terminators.
The BMXXBE2005 is an Extension rack kit that contains everything that you need including:

  • 2 BMXXBE1000 extension rack modules
  • one BMXXBC008K 0.8 meter extension cable
  • one TSXTLYEX set of 2 line terminators

Other cable lengths available:
BMXXBC015K - 1.5m extension rack cable.
BMXXBC030K - 3m extension rack cable.
BMXXBC050K - 5m extension rack cable
BMXXBC120K - 12m extension rack cable

Schneider Electric Canada

Attachment(s)
Rack Expansion.pdf [324.21 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings