Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION7600 Meter Template Files

Product Line
ION7600

Environment
Templates

Resolution
You can install meter templates using ION Setup. See the "Upgrading ION Device Firmware" technical note for complete details.

Install Templates with ION Setup:

  1. Download the device template and save it to your ION Setup TEMPLATE folder (select the file below that matches your meter's feature set).

Use these .DCF files with ION Setup to perform firmware upgrades. These are default meter templates only. If you have custom programming in your meter, create your own template file before performing the firmware upgrade.

  1. Follow the upgrade procedures outlined in the Upgrading ION Device Firmware technical note.


Attached below you will find the ION Setup Meter Templates for firmware V250- V254:

1 Amp (Class 2): 7600_v250_FAC-4WYE_V1.5.0.0.3

5 Amp (Class 20): 7600_v250_FAC-C2A-4WYE_V1.5.0.0.3

Schneider Electric Canada

Attachment(s)
7600_v250_FAC-C2A-4WYE_V1.5.0.0.3.dcf.zip [89.08 KB]
7600_v250_FAC-4WYE_V1.5.0.0.3.dcf.zip [89.06 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings